AXIS#.VL.VFTHRESH
Description
This parameter reports the overall overspeed fault threshold. The following thresholds with the smallest value is used as the overall overspeed fault threshold:
- User overspeed threshold (AXIS#.VL.THRESH).
- Motor mechanical overspeed threshold (1.2 x AXIS#.MOTOR.VMAX)
- Motor back EMF overspeed threshold ((1.02 x 1000 x VBUS.OVFTHRESH) / (AXIS#.MOTOR.KE x sqrt(2))).
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read Only |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
Float |
|
Stored in Non-Volatile Memory |
No |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.VL.VFTHRESH |
5011h |
2dh |
Signed32 |
- |
1000:1 |
Read only |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
6036 |
1 |
6036 (0x1794) |
AXIS1.VL.VFTHRESH |
Signed32 |
Read Only |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS1.VL.VFTHRESH |
6036 |
Float |
Read Only |
Velocity |
Related Topics